This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS2200: Surge Clamp Characteristics

Part Number: TVS2200

Dear Team,

My customer is evaluating the TVS2200DRVR to clamp surge on AC Adapter input line of  VIN=19.5V.
They would like to know the following characteristics of surge clamp of the TVS2200.

1) Is there a characteristic diagram showing the relationship between temperature and clamp voltage?

2) If the pulse is shorter than IEC 61000-4-5 Surge (8/20 us), is there anything they should be aware of?
    As a result of their evaluation, the actual measurement is about 1.5/3 usec, and the maximum current value is 15A.

3) Is there a limit to the number of surges when used within the specified limits (e.g. 20A)?

4) When using a TVS2200 suege protection device as an anti-inrush like this time, is there anything to be aware of in the layout?

Best Regards,

Koshi Ninomiya