Other Parts Discussed in Thread: TUSB7340
Hi, we are using the TUSB7320 USB 3.0 Host in a prototype design. The chip connects to a
PCIe Gen 1 host (chipset ICH8M) on our board. When booting both Ubuntu 11.10 and Windows
XP, the OS can see the TI PCIe target device. However, our crystal circuit does not oscillate ever.
Our design is closely based on the TUSB7320 EVM. A 1 MOHM resistor is placed across XO
and XI. 18 pF capacitors are placed between XO, XI and VSSOSC. We are not using the optional
EEPROM and both SDA and SCL are grounded. The FREQSEL pin is grounded. We have a clean
deassertion of RST# after power supplies are stable. PCIe Ref Clk is stable before the PCI Reset
is deasserted by the host.
In addition, we have tested the same crystal used in the TUSB7320 EVM reference design as well
as a slightly different one (Abracon ABLS-48.00MHZ-B2-T) on multiple boards ruling out faulty crystals.
So, we are wondering if the crystal is supposed to be oscillating when first powered (as we suspect) or
only when it sees a USB device on the hub?
Any help would be appreciated.
Thanks,
Patrick