Part Number: DS160PT801
Hi,
We are debugging a low temperature(near -40C) failure. Seems to be downstream receivers.
We can see one lane margin dithering over time from good to small. We do not believe the transmitter is varying - Only the retimer end is at low temperature.
I do realize in general the guidance is that auto tuned is best. Just trying to nail down the failure by over-riding.
We ar efinding that the FSM seems to keep adjusting...
Refs end up -64,+64 and DFE tap1 moves to the extreme. And if we apply the overrides before link training, it links gen1, but doesn't seem to attmept to advance to next speeds.
We are setting: Ov_en and value in 0xC3, Value in C4, ov_en and value in C5,C6
Tried also: Reg 0x58: The suggested EEPROM file value, as well as masking DFE
Also, reg 0xB6, all combinations of bits 2 and 3
Any advice is appreciated.