Part Number: DS110DF111
Hello ,
We are currently using a custom developed board based on NXP's LX2160 network processor. We are testing 10G interface on the same which involves a DS110DF111 retimer in between an SFP+ cage. When we try to bring up the link in LX2160 linux we are not able to see any link comming up. Next we bypassed the retimer and tried the same now the link comes up but seems to be somewhat unstable. We are able to send packets too.
My question is, with retimer in place do we need to write anything into it to bring the link up. As per datasheet its mentioned that by default it's channels are set to 10.3125 Gbps which is a required criteria in our case for 10Gbps. Can you tell me what else we are suppose to do on the retimer?