Part Number: LMH0397
Hello E2E Experts,
We're using LMH0397 to output DVB-ASI signal.On our board,there're 8 ASI channels and each one using one LMH0397.In the test of output eye diagram, we found that the jitter performance of some of these channels is poor,with jitter values reaching 400~500ps,while the normal channels are approximately 200ps.The screenshot is as follows.
Good channel:

Bad channel:

As we've tried all possible debugging steps per AE's suggestiongs without improvement,finally we tried to bypass the CDR module inside the LMH0397.Unexpectedly, the test result of jitter is less than 100ps, better than those with CDR enabled.
jitter with CDR bypassed:

I haven't found much descriptions about transmitting DVB-ASI signal in the LMH0397's datasheet Could you please answer the following questions?
(1)Is it a normal situation that the LMH0397 has additional jitter when transmitting DVB-ASI signals with CDR enabled?
(2)If yes,why do some of them have nearly 500ps of jitter while most of others only have 200ps?
(3)If not,are there any settings in the LMH0397's registers can improve the jitter performance?