Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1029-Q1: pull up resistance limitation

Part Number: TLIN1029-Q1

Hello expert,

May I know if there is limitation for TLIN1029-Q1 pullup resistance? When we use 10kohm or 30kohm, is that any impact for communication? Thanks a lot!

Best regards,

Ann Lien

  • Hi Ann,

    Our LIN transceiver already integrates a 45K Ohm pullup for responder node application, so there is no need to add external pullup.

    For commander node application 1K Ohm is required by the LIN standard, to ensure a fast enough rising edge. There is no reason to use other value resistors.

    Regards,

    Sean