Part Number: TUSB8044A
Other Parts Discussed in Thread: TPS2559
Hello TI Support Team,
My name is Mihir Chauhan and I am working at Aimtron Technologies as a Senior Hardware Design Engineer.
Currently I am working on a new project which is in the design phase. We have to design a USB hub using the TUSB8044A from TI, which must support downstream ports of Type-C USB 3.2 and must be able to charge a device at 5 V and 4 A. The hub will also need power-distribution control and current limiting, for which we are considering the TPS2559 power-switch/current-limit controller from TI.
In this context, is it necessary to connect a PD (Power Delivery) controller to the downstream Type-C port in order to support charging at 5 V and 4 A? Or can we simply use pull-resistors on the CC pin of the Type-C interface to advertise the required current draw (4 A) and rely on the hub’s power-distribution switch (TPS2559) and hub controller (TUSB8044A) to manage the power safely?
Thank you for your support and guidance.
Best regards,
Mihir Chauhan