This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: Possible Datasheet Typo

Part Number: SN75DP130

Hello Please refer to Section 7.3- Recommended Operating Conditions

 

For V IH and V IL, 

V IH has a range of 1.9V - 3.6V, but the nom RST pin voltage is listed as 0.75V, which is not in the 1.9 - 3.6V range whatsoever. 

 

V IL has a range of 0 - 0.8V, where nom is 0.3V, which does nicely fall into that nominal range. 

 

Please let us know as we are trying to correct our design. This is very very confusing. 

 

 

Screenshot 2025-11-12 144119.png