This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9548A-Q1: TCA9548A and TCA9548A-Q1 operating temperature

Part Number: TCA9548A-Q1
Other Parts Discussed in Thread: TCA9548A,

Hello,

I have a few questions about TCA9548A and TCA9548A-Q1 (Automotive).

In TCA9548A datasheet (SCPS207H-revised September 2024), it is indicated :

  • Ta - Operating free-air temperature – 3.6 V ≤ VCC ≤ 5.25 V  -40/+85°C + Tj max 90°C
  • Ta - Operating free-air temperature - 1.65 V ≤ VCC ≤ 3.6 V  -40/+125°C + Tj max 125°C

In TCA9548A-Q1 datasheet (revised June 2023), it is indicated :

  • Ta - Operating free-air temperature - 1.65 V ≤ VCC ≤ 5.25 V  -40/+85°C + Tj max 90°C
  • Ta - Operating free-air temperature - 1.65 V ≤ VCC ≤ 3.6 V -40/+125°C + Tj max 125°C

In TCA9548A-Q1 datasheet, the voltage at -40/+85°C should not be rather 3.6 V ≤ VCC ≤ 5.25 V ?

If the operating free-air temperature are the same, what is the difference between these 2 réferences ?

Thanks,