Part Number: ESD2CANFD24-Q1
Hi expert
Please can you offer the capacitance difference between the two branches for the CAN bus?
In the datasheet, I only find the line capacitance as below
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ESD2CANFD24-Q1
Hi expert
Please can you offer the capacitance difference between the two branches for the CAN bus?
In the datasheet, I only find the line capacitance as below
Hi Song lin,
Are you asking for capacitance between Pin 1 to Pin 2?
Best,
Bryan
Hi Bryan
I mean the ΔCd, which is the difference of the capacitance measured between pin 1 and pin 3 and the capacitance measured between pin 2 and pin 3.
The question similar to below ,but different MPN. Can you also offer the percent? which is ΔCd/Cd.

Hi Song,
Thanks for explaining the question. Diode capacitance matching (VIO=0V, f=1MHz, Vp-p = 30mV) is 0.5%.
Let me know if you need anything else.
Best,
Bryan