Part Number: TMUXHS4212
Hi Team,
Please help to check if there is any problem for the design?
Customer found the speed cannot up to USB2.0 and USB3.0!
Thanks for the helping.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUXHS4212
Hi Team,
Please help to check if there is any problem for the design?
Customer found the speed cannot up to USB2.0 and USB3.0!
Thanks for the helping.
Hi Peter,
I am not seeing any major concerns upon first glance. A few suggestions - you only need capacitors on one side of the switch, so you can remove C5293&C5294.
Could you clarify which power source is being used for VCC? Right now, the schematic shows two options (VDD3V3 & VIO18_PMU). There should only be one connected. Additionally, the RSVD pins are ok as long as VCC is tied only to VIO18_PMU. If VCC is tied to VDD3V3, the RSVD pins also need to be tied to VDD3V3.
It is unclear from the original post if the customer is just requested a schematic review or is actually seeing an issue. If they are seeing an issue, could you please give specifics (voltages used, scope shots, what pins are seeing issues)?
Thanks!
Katy