This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXE8124-Q1: TXE8124

Part Number: TXE8124-Q1

Hi, TI Experts

Question 1: as picture shows below , Is there Clamp Diode between GPIO Pin to VCC ?

( Does the IC has the ability to clamp the input voltage to VCC+04V?)

Question 2:

If all the IC GPIOs are used for GPO output function , Does the INT pin make sense?  Is the INT pin floating ?

Thanks !

 

  • Hi Bin,

    Question 1: as picture shows below , Is there Clamp Diode between GPIO Pin to VCC ?

    ( Does the IC has the ability to clamp the input voltage to VCC+04V?)

    I measured the P00 pin to VCC on a multi-meter with the diode function and got 1.7V. 

    The recommended operating conditions in the datasheet suggest that VIH should be max VCC and not over. 

    Question 2:

    If all the IC GPIOs are used for GPO output function , Does the INT pin make sense?  Is the INT pin floating ?

    You can have /INT pin floating as this pin is an open-drain output. 

    Regards,

    Tyler