Other Parts Discussed in Thread: TCA9406
Hi,
I am a student of Robotics at Plymouth University, England. I am currently attempting to integrate an IR range finder onto a PCB with an 8-bit YUV Camera, the camera's output voltage level is 2.5V, which in turn is connected to an Altera Cyclone II FPGA. I have had to use a 5V power supply for the IR range finder, the output is then converted to a digital signal and I intend on using the TCA9406 to translate the 5V digital signal to a 2.5V digital signal to then be output from the PCB to the FPGA as well.
My problem is that the data sheet for the TCA9406 explains that there are different rise times for Push-Pull and Open-Drain configurations, but it does not tell me how to determine which I am using. I believe the rise times to be of significance because (from my understanding) the input port is selected by powering it before the desired output port. I need to calculate a suitable CR time delay for port A.
Any explanation or help would be greatly appreciated.
Thank you for your time.
James