Part Number: SN75LVPE5412
Hello:
PN#SN75LVPE5412RUAT
1. Can two SN75LVPE5412 be connected in series from RC to EP for PCIe Gen5 applications?
2. For a link from RC to EP, if half of the lanes have SN75LVPE5412 strung on them and half of the lanes do not, is there a problem with this application?
3. Regarding the protocol, is the chip SN75LVPE5412 transparent?
Thanks!!!