This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Design review

Guru 13005 points

Part Number: DP83867IS

Hello,

My customer requested TI's review of the circuit for the DP83867ISRGZ.

Please review the customer's circuit below to ensure there are no problems.

TI_PHY_DP83867ISRGZ.pdf 

Additionally, does the DP83867ISRGZ have MDI Auto polarity functionality? Is it correct for users to enable Mirror mode for MDI Auto polarity?

image.png

Thank you.

  • Hi JH, 

    Below are my comments:

    1. Please ensure MDIO has a pull-up to VDDIO. 
    2. 
    Is there a reason why R44 has 150ohm resistor?


    Additionally, does the DP83867ISRGZ have MDI Auto polarity functionality?

    DP83867 does not have auto polarity detection functionality. In mirror mode, polarity is flipped. 

    In addition, the customer can refer to our schematic checklist if they want to check on their own also. 

    Best,
    J