Part Number: SN65EPT21
Other Parts Discussed in Thread: SN65EPT22
Good Morning.
I'm using SN65EPT21 receiver, powered through +3,3V power supply +/- 100mV.
SN65EPT21 inputs are connected to a transformer and middle of the transformer is connected to VBB. A 200 ohm differential resistor is present between D and /D. AC input signal injected through the transformer's primary and SN65EPT21 output is responding well.
But when I have no connexion on the transformer's primary, I can see the output which is oscillating. As It is indicating on the datasheet descritpion : "The device includes circuitry to maintain inputs at Vcc/2 when left open". As the input may have the same voltage level, why output is oscillating ? Does power supply may be the cause of the oscillation ?
Thanks per advance for your answer.
Sincerely,
Vincent