Part Number: SN65DSI83
Hello,
We are testing the SN65DSI83 MIPI DSI to LVDS bridge with a display (datasheet attached). The converter is connected to an SC200E module running Android 14. We have a custom driver that writes the I²C registers to the SN65DSI83.
To validate the connection between the display and the converter, we configured the device to output the LVDS test pattern. However, we do not see any pattern on the screen.
We are attaching:
- The display datasheet 250606 7 inch Panel - Datasheet (1).pdf
- Our driver implementation mipi_convert.c
- The register configuration from DSI Tuner test_mode.txt
Additional details:
- We tried changing register 0x1A to value 0x01 (100ohm differential termination), but the issue persists.
- I think the driver logs look correct and indicate that the I2C writes are successful:
bengal:/ # dmesg -w | grep convert [ 5.194323] convert_probe, Start [ 5.199539] mipi_convert 0-002c: convert_parse_dt: Pincontrol DT property failed [ 5.247071] mipi_convert 0-002c: 0-002c supply avdd not found, using dummy regulator [ 5.254936] mipi_convert 0-002c: Linked as a consumer to regulator.0 [ 5.261317] mipi_convert 0-002c: convert IC probe success [ 5.266741] mipi_convert 0-002c: init convert IC ... [ 6.344369] mipi_convert 0-002c: reg: 9, READ8: 0 [ 6.344609] mipi_convert 0-002c: reg: a, READ8: 85 [ 6.344848] mipi_convert 0-002c: reg: b, READ8: 10 [ 6.345085] mipi_convert 0-002c: reg: d, READ8: 1 [ 6.345323] mipi_convert 0-002c: reg: 10, READ8: 26 [ 6.345561] mipi_convert 0-002c: reg: 11, READ8: 0 [ 6.345800] mipi_convert 0-002c: reg: 12, READ8: 2a [ 6.346039] mipi_convert 0-002c: reg: 13, READ8: 0 [ 6.346276] mipi_convert 0-002c: reg: 18, READ8: 78 [ 6.346514] mipi_convert 0-002c: reg: 19, READ8: 0 [ 6.346752] mipi_convert 0-002c: reg: 1a, READ8: 1 [ 6.346989] mipi_convert 0-002c: reg: 1b, READ8: 0 [ 6.347227] mipi_convert 0-002c: reg: 20, READ8: 0 [ 6.347465] mipi_convert 0-002c: reg: 21, READ8: 5 [ 6.347702] mipi_convert 0-002c: reg: 22, READ8: 0 [ 6.347940] mipi_convert 0-002c: reg: 23, READ8: 0 [ 6.348181] mipi_convert 0-002c: reg: 24, READ8: 20 [ 6.348420] mipi_convert 0-002c: reg: 25, READ8: 3 [ 6.348659] mipi_convert 0-002c: reg: 26, READ8: 0 [ 6.348896] mipi_convert 0-002c: reg: 27, READ8: 0 [ 6.349135] mipi_convert 0-002c: reg: 28, READ8: 21 [ 6.349372] mipi_convert 0-002c: reg: 29, READ8: 0 [ 6.349612] mipi_convert 0-002c: reg: 2a, READ8: 0 [ 6.349850] mipi_convert 0-002c: reg: 2b, READ8: 0 [ 6.350088] mipi_convert 0-002c: reg: 2c, READ8: 50 [ 6.350326] mipi_convert 0-002c: reg: 2d, READ8: 0 [ 6.350563] mipi_convert 0-002c: reg: 2e, READ8: 0 [ 6.350801] mipi_convert 0-002c: reg: 2f, READ8: 0 [ 6.351039] mipi_convert 0-002c: reg: 30, READ8: a [ 6.351276] mipi_convert 0-002c: reg: 31, READ8: 0 [ 6.351515] mipi_convert 0-002c: reg: 32, READ8: 0 [ 6.351752] mipi_convert 0-002c: reg: 33, READ8: 0 [ 6.351991] mipi_convert 0-002c: reg: 34, READ8: 28 [ 6.352231] mipi_convert 0-002c: reg: 35, READ8: 0 [ 6.352469] mipi_convert 0-002c: reg: 36, READ8: 14 [ 6.352707] mipi_convert 0-002c: reg: 37, READ8: 0 [ 6.352945] mipi_convert 0-002c: reg: 38, READ8: 28 [ 6.353183] mipi_convert 0-002c: reg: 39, READ8: 0 [ 6.353421] mipi_convert 0-002c: reg: 3a, READ8: a [ 6.353658] mipi_convert 0-002c: reg: 3b, READ8: 0 [ 6.353896] mipi_convert 0-002c: reg: 3c, READ8: 10 [ 6.354135] mipi_convert 0-002c: reg: 3d, READ8: 0 [ 6.354372] mipi_convert 0-002c: reg: 3e, READ8: 0 [ 6.354610] mipi_convert 0-002c: reg: d, READ8: 1 [ 6.372320] mipi_convert 0-002c: reg: 9, READ8: 0 [ 6.392082] mipi_convert 0-002c: End of convert_init [ 8.424484] mipi_convert 0-002c: reg: e5, READ8: 25 [ 10.440492] mipi_convert 0-002c: reg: e5, READ8: 0 [ 12.456496] mipi_convert 0-002c: reg: e5, READ8: 0 [ 14.479241] mipi_convert 0-002c: reg: e5, READ8: 0 [ 16.531441] mipi_convert 0-002c: reg: e5, READ8: 0 [ 18.600477] mipi_convert 0-002c: reg: e5, READ8: 0 [ 20.616473] mipi_convert 0-002c: reg: e5, READ8: 0 [ 22.632504] mipi_convert 0-002c: reg: e5, READ8: 0 [ 24.648499] mipi_convert 0-002c: reg: e5, READ8: 0 [ 26.664560] mipi_convert 0-002c: reg: e5, READ8: 0 [ 28.681645] mipi_convert 0-002c: reg: e5, READ8: 0 [ 30.697030] mipi_convert 0-002c: reg: e5, READ8: 0 [ 32.713776] mipi_convert 0-002c: reg: e5, READ8: 0 [ 34.728522] mipi_convert 0-002c: reg: e5, READ8: 0 [ 36.744504] mipi_convert 0-002c: reg: e5, READ8: 0 [ 38.760907] mipi_convert 0-002c: reg: e5, READ8: 0 [ 40.776600] mipi_convert 0-002c: reg: e5, READ8: 0 [ 42.792595] mipi_convert 0-002c: reg: e5, READ8: 0 [ 44.810617] mipi_convert 0-002c: reg: e5, READ8: 0 [ 46.824672] mipi_convert 0-002c: reg: e5, READ8: 0 [ 48.844633] mipi_convert 0-002c: reg: e5, READ8: 0 [ 50.856620] mipi_convert 0-002c: reg: e5, READ8: 0 [ 52.875207] mipi_convert 0-002c: reg: e5, READ8: 0 [ 54.888890] mipi_convert 0-002c: reg: e5, READ8: 0 [ 56.905806] mipi_convert 0-002c: reg: e5, READ8: 0 [ 58.920638] mipi_convert 0-002c: reg: e5, READ8: 0 [ 60.936559] mipi_convert 0-002c: reg: e5, READ8: 0 ...
Could you please help us identify why the test pattern is not appearing?
Thank you for your support.
Hanwei