Part Number: TL16C752D
Other Parts Discussed in Thread: THVD1500, THVD1406
Hello guys,
One of my customers is considering using TL16C752D for their new products.
At this moment, they have the following questions.
Could you please give me your reply?
Q.
They want to convert signals between UART and RS485
because their CPU doesn't have RS-485 port and have UART port only.
Their product is connected to a device which has RS485 interface.
So they are looking for a device which can convert signals beteen UART and RS485.
Can TL16C752D convert signals between UART and RS485?
(Of course, they know a RS485 tranceiver,(ex. THVD1500) is needed to connect to external device).
Your reply would be much appreciated.
Best regards,
Kazuya.