Part Number: TMUXHS4446
Other Parts Discussed in Thread: TUSB8041, , TPS65987
Hi TI:
We are designing a monitor with Type-C as the UFP interface, using 4446 and 65987. Please help confirm the schematic. The main uncertainties are as follows:
1. Whether the connections for CTX1, CTX2, CRX1, and CRX2 are correct;
2. Whether the SBU1 and SBU2 swapping is correct;
3. Whether the connections for Pin 11, 12, 16, and 17 to the USB HUB (TUSB8041) are correct, and whether capacitors are needed between them;
4. For control mode using GPIO without I2C, can MODE0, MODE1, and A0 be connected to ground?
Also, are there any reference documents similar to our application that you would recommend?
Best Regards
Eric