This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9517A: Can side-B be powered off while side-A is high?

Part Number: TCA9517A

Hi,

I am evaluating using TCA9517A as I2C buffer, between two modules powered by 3.3V, but one side (A) is constantly powered while the otherside (B) can be powered off.

TCA9517A 's datasheet says

  • High-impedance I2C pins when powered-off
  • VCCB and VCCA can be applied in any sequence at power up. The TCA9517A includes a power-up circuit that keeps the output drivers turned off until VCCB is above 2.5V and the VCCA is above 0.8V.

But on the product page, it says "Supply restrictions VCCA <= VCCB ".

  • Does that mean, VCCB cannot be powered off while VCCA?
  • What are the requirements to achieve high-impedance on I2C pins?

Otherwise, could you please suggest any alternative for this requiement?

Thanks!

  • Hello,

    Today is a US National Holiday, as a result, responses may be delayed. Thank you for understanding!

    Regards,

    Jack

  • Hi Js,

    This device supports high-z i2c pins when powered off, this includes the condition VCCA = ON, VCCB = OFF. 

    The product page says supply restrictions VCCA <= VCCB, this is during the recommended operating of the device. When in an OFF state, VCCA and VCCB can be powered in any sequence. 

    Regards,

    Tyler