Part Number: TUSB320
Other Parts Discussed in Thread: LM66100, , TUSB321
Hello there,
We are making a USB C audio dongle with charge through capability. It will be a simple female USB C power constantly requesting 5V by 5.1k resistors on its CC lines. This power will go through a LM66100 ideal diode into the SYS_5V. The SYS_5V should connect to the cell phone's USBC male plug VBUS lines and also to the DAC/ADC peripheral. When the external female plug is unconnected, the TUSB320 should set the phone as UFP, requesting power from the phone. When VBUS detects power from the female power, the TUSB320 should switch the phone to DFP and receive charge from the external charger. In each case the DAC/ADC peripheral should remain powered.
Our question is, should the VBUS_DET monitor the external power bus or the VSYS_5V bus?
Additionally, is it okay that LM66100 remains constantly "ON"? Or must its enable be controlled by the TUSB320 ID pin?
Could you review schematic and advise?

Thank you,
Peter