This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: Clarification on Temperature Range for HS4212 Component

Part Number: TMUXHS4212

Dear Texas Instruments Support Team,

I am working with a component marked as:

HS4212
TI 478
AY29

I believe this corresponds to the TMUXHS4212 family. Could you please confirm the following:

  1. Is this marking associated with the commercial grade (0°C to 70°C) or the industrial grade (−40°C to 105°C)?
  2. Are there any additional identifiers in the lot code that indicate temperature grade?
  3. Could you provide any official documentation or guidance on interpreting these markings?

Thank you for your assistance.

Best regards,