Part Number: DS250DF410
Hi expert,
May I have your help on below question?
- Do you have any design guides, reference schematics/layouts, or layout guides that you can provide?
2. According to the datasheet, the external EEPROM I²C address must be set to 0xA0. If the address is set to a different value, will the retimer still function correctly?
3. Please help confirm whether this is correct:
MAX Power consumption = 2.5 V × 665 mA = 1.663 W
4. Please provide the thermal model for simulation.
Thanks a lot!
Jenny