Part Number: DS80PCI402
Dear Technical Support Team,
I am planning to use the DS80PCI402 in a new design and I would like to confirm two technical points.
1. Differential pair swapping within the same channel group
For layout reasons and to better match my pinout, I would like to know whether it is allowed to swap differential pairs within the same group/channel, as long as the polarity (N/P) is preserved.
For example, can the pair Tx_0_N / Tx_0_P be routed instead to Tx_3_N / Tx_3_P, and vice-versa?
Please confirm whether such internal channel swapping is electrically acceptable for the DS80PCI402, or if each differential pair must be routed strictly to its corresponding pins.
2. Use of AC-coupling capacitors on TX/RX lines
In the datasheet and on the official evaluation board, AC-coupling capacitors (0.22 µF) are placed in series on the TX and RX differential pairs.
Is this also recommended in a scenario where the DS80PCI402 is located on a backplane, and both plug-in boards connected to the backplane already include their own AC-coupling capacitors on the same differential links?
In other words, should additional capacitors be placed on the backplane near the DS80PCI402, or should they be omitted to avoid multiple series capacitors on the same lane?
Thank you in advance for your support.
Best regards, Adrian