This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: issue with the top marking of DP83826ERHBR

Part Number: DP83826E

image.png

The DP83826ERHBR Ethernet PHY used on our boards exhibits different functional behavior depending on the top marking of IC. Units assembled with PHY devices marked:

  • 826E TI 298 AS7Y G4 → functioning normally

  • 826E TI 198 ALRX G4 → failing to operate,

    • What do the different top markings (AS7Y vs ALRX) represent?

    • Do these marking codes indicate different manufacturing lots, revisions, or device versions?

    • Could the marking difference be related to the observed functional difference?

    • Are there any known functional or behavioral differences between these units ?

  • Hi Dona,

    DP83826 had a revision change during the pandemic. There can be a chance this is one of those ICs. Could you read the PHYIDR2 (reg 03h) register of the not working chip? Bits 0 to 3 hold the revision number information.

    Best,

    J