Part Number: LMH0397
Hi,
We are using LMH0397RTVT 3G SDI Equalizer & Cable driver in our design.
1) The differential standard of IN+, IN-, OUT+ & OUT- pins are not mentioned in the datasheet.
Which differential standard does this chip support (CML or LVDS or any other standard)?
2) We are planning to interface this chip with MGT bank of AMD FPGA. Can we interface with FPGA MGT Bank?
3) Also confirm max data rate of this high speed differential interface of LMH0397.
4) If we use Belden 1694A cable, How much distance and data rate does it support for 3G SDI Interface?
5) Is there any other concerns we need to look into for using this chip for 3G SDI Interface?