Part Number: TUSB8041
Other Parts Discussed in Thread: TPS2561
Hi Teams,
My customer has a project where they used TUSB8041+TPS2561 for a HUB application. Occasionally, when the device is powered on, the PWREN output of 8041 is not pulled high, resulting in the VBUS of the downstream port running out of power.


This is a testing device, and the feedback from end customers was initially positive. However, this issue occasionally occurred while using it. At first, they thought it was ESD causing damage to the VBUS switch, but after replacing the chip with ABA, they found that the function was normal. Then they suspected the current limiting protection again, and checked that the fault pin on the dead side was not pulled down, it was the PWREN of the HUB that was not pulled up.
The following is the waveform of the test. Blue represents VDD 1.1, yellow represents fault, and purple represents PWREN.

After being powered on for about 4 seconds, PWREN pulled down.
Please help analyze the cause of the problem and provide some suggestions. Thank you~