This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1142: About the CEQ and SSEQ setting on TUSB1142

Part Number: TUSB1142


Hi AE,

      The current Pre-Channel total and Post-Channel total are as follows.

      Could you help recommend the appropriate settings for CEQ1, CEQ0 and SSEQ1, SSEQ0?  

Type C Gen2 CEQ1 CEQ0 SSEQ1 SSEQ0 AEQENZ AEQCFG Pre-Channel total Post-Channel total
FIO Type C Gen2 #1 Retimer 1142 0 0 R R F 0 2427.77 1058.04
FIO Type C Gen2 #2 Retimer 1142 0 0 R R F 0 3106.52 1029.76
RIO Type C Gen2 #1 Retimer 1142 0 0 R R F 0 10327.83 735
RIO Type C Gen2 #2 Retimer 1142 0 0 R R F 0 10972.45 661.44

 

Best Regards

  • Hi,

    If you are using the TUSB1142, it's best to use the AEQ function of the part to determine the best EQ for the post channel.

    Based off of the chart provided, I am understanding that there are 4x TUSB1142 devices on the system.

    FIO redriver #1: SSEQ level 0-2, AEQ for post channel

    FIO redriver #2: SSEQ level 0-2, AEQ for post channel

    RIO redriver #1: SSEQ level 7-15, AEQ for post channel

    RIO redriver #2: SSEQ level 7-15 AEQ for post channel