This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS110DF111: Ds110df111 info

Part Number: DS110DF111

Hello TI experts. I need to know if the ds110df111 3R device supports the Xilinx AURORA 64/66b 10 Gbps ( 10.3 Gbps raw bitrate) protocol.

  • Hi Luca,

    The DS110DF111 is not a protocol aware device, so it doesn't have a strict protocol dependency.  10 GbE is also 64/66b encoded and has 10.3125 Gbps line rate.

    Assuming signaling levels of Xilinx Aurora are comparable to typical Ethernet signal (typically 600mVppd - 1600mVppd), I would not expect any issues with DS110DF111.

    Thanks,

    Drew