Part Number: TCAN4550
Hi, we have a product that uses TCAN4550 that is well-tested and everything functions as intended.
We have just begun Radiated Emissions testing and we are failing because of excessive emissions in the harmonics of 40Mhz (120, 200, 280 etc). We have pinpointed the 40Mhz TCAN crystal as the source of the emissions. We hope that by making small changes to our board we can reduce these emissions.
- Our original design is a little lacking in coupling capacitors for the TCAN chip. is it possible that adding capacitance could reduce noise in the system?
- We are seeing that our CAN wires radiate this same noise. We chose not use a choke between CANH and CANL due to packaging constraints. Assuming we are able to reduce the noise from the crystal, can we get away without a choke here? If not, is there a very small choke you could recommend?
- We chose to use OSC1 as an external clock input and we grounded OSC2. The datasheet shows a crystal oscillator connected to both OSC1 and OSC2. Can you outline the differences between these two approaches?
- Is it possible to use a "damping resistor" on the oscillator to reduce emissions while still allowing the TCAN to function properly?