This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD4431: THVD4431EVM not working as expected

Part Number: THVD4431

Team,
Could you please help with the below request?

This card is not functioning as expected:
   -Board powered by 5V (V+ is approximately 5V and V- is -3V).
   -we configured it in mode 001 (RS232) and looped L2 back to L3.
See attached pics of card configuration and oscilloscope measurement with R2 on channel 1 and R3 on channel 3. 
-Why don't we see the same signal on both channels?

We ultimately want to power the board with 3.3V, but then we measure V+ at 3.2V and V- at 700mV.
-Is this behavior expected?

THVD4431EVM_jumpers.png

RS232_R2-R3.jpg

 

Thanks in advance,
Anber