Part Number: TCAN1462-Q1
Hi TI Team,
I am currently designing a new system in which we use CAN-FD to communicate between system components. The bus is strictly for internal use and does not need to interface with external or third-party CAN devices.
Since we require some external cabling to connect the different system components, we would like to use standard Ethernet cables. We currently use two 60 Ohm resistors with a 4.7 nF capacitor as the termination and the TCAN1462-Q1 as transceiver.
Is it possible to terminate the bus with 50 Ohm instead, in order to match the characteristic impedance of Ethernet cables?
Thank you in advance.
Best regards,
Theo