Other Parts Discussed in Thread: SN65HVD21, SN65HVD24, SN65HVD20, RS485-HF-DPLX-EVM
Hi,
Looking to use the SN65HVD23 in an application where continuous data is being sent unidirectionally through up to 200m of shielded twisted pair at up to 10 Mbit/sec. Page 21 of the datasheet, section 10.4.1 Test Mode Driver Disable, states:
If the input signal to the D pin is such that:
1. the signal has signaling rate above 4 Mbps (for the SN65HVD21 and SN65HVD24),
2. the signal has signaling rate above 6 Mbps (for the SN65HVD20 and SN65HVD23),
3. the signal has average amplitude from 1.2 V to 1.6 V (1.4 V +/- 200 mV), or
4. the average signal amplitude remains in this range for 100 us or longer,
The input D pin will be connected to a FPGA where Vhigh-Vlow/2 would be around 1.3V and the waveform (from a serializer) can be expected to average a 50% duty cycle. Data is sent continuously.
In initial testing of the part (using a pair of RS485-HF-DPLX-EVM) and a 10 MHz 50% duty cycle clock output failure due to test mode was not observed, but also may have not noticed occasional dropouts.
Subsequent testing used a 3 Mbit/sec rate as the initial system design will use that rate. A future upgrade will increase that about three times, hence the 10 Mbit/sec design allowance.
If I've read the section 10.4.1 description correctly then the SN65HVD23 can't be used above 6 Mbps even though the product description says it supports up to 25 Mbps.
If 10.4.1. is correct and the part is limited to 6 Mbps due to the test mode is there a part that can support 200m of cable at 10 Mbps? Or is there some way to prevent entering test mode under the operating conditions we have? Figure 11-2 shows the part running at 25 Mbps so I'm hoping I have misunderstood what 10.4.1 is saying.
Thanks,
Brewster