Part Number: TCAN1145-Q1
Hi team,
Could you help on below questions from TCAN1145 wakeup?
- Since the interrupt events will impact state transition, for example UCIO, UVCC, TSD etc. If don’t want this states impact state machine transition, could they just disable them in ENABLE register? or this only impact nINT behavior but doenst input state transition
- What is the recommended configuration for INT ENABLE? The requirement is MCU use SPI to control TCAN1145 enter normal and sleep mode, and related selective wakeup. Which registers in INT_ENABLE1,2,3 need to be configured?
- Before entering sleep mode, should customer W1C all INT1,2,3?
- Is there any way to disable local wake up?
Thanks
Scarlett