Part Number: LMH0387
Hi Team,
Can you advise me on my questions bellows:
On page 18 of the LMH0387 datasheet stats that, the register address 02h bit 6 through 3 set the Launch Amplitude Fine Control. The default value is 0110 for Nominal Launch Amplitude.
Q1. When the value in bit 6:3 either decrease or increase, the index is signed as plus (+) except 0111 (-2%) case. Are the setting 1001 to 1111 index are -24% to -60 % Instead of +24% to +60%?
Q2. When bit 6:3 is set 0000 (+20%), the device is optimized to handle the input, which Launch Amplitude is 960 mV (800 +20%) (or 480mV: 400+20% if bit7 =1)?
Mita