Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: TI960 connection status register

Part Number: DS90UB960-Q1

Hi 

     TI960 can connect four ti953 serialziers. Any register from TI960 side can be read to indicate which port is connecting serializer and which is not?

 

Thanks

Xingxing

  • Hi Xingxing, 

    For diagnostics on the UB960, we recommend reading back register 0x4D, 0x4E, 0x55-0x56, and 0x7A-0x7B. These registers are port specific. To select the port to read from, please select the RX port in register 0x4C[5:4]. Errors may be flagged in these registers during start up and are recommended to be cleared first via read-back. LOCK is reported in 0x4D[0]. PASS criteria can be set in 0x7D. By default, the PASS criteria will follow the lock status. PASS is read back via 0x4D[1]. 

    Best,

    Zoe