Part Number: LSF0204-Q1
Other Parts Discussed in Thread: LSF0204
Our partner company is about to implement the circuit shown below.
Please allow me to confirm the following 1 to 3.
Thank you in advance.
1. Logic level of Signal_A1
If Signal_B1 is High by pull-up(R3), will Signal_A1 be 1.8V in this circuit?
Background: Originally there was a pull-up instead of C1, but they are trying to replace the resistor with C1 to prevent overshoot when Signal_A1 goes from Low to High. The purpose is to channel the high frequency component of the overshoot to the power supply.
2. Logic level of Signal_B2
Signal_A2 has a pull-down and Signal_B2 has a pull-up.
Is it possible to prevent intermediate voltage due to resistive voltage divider as long as the source device is outputting High/Low with sufficient drive strength?
3. Behavior while Vref_B is turned on and the voltage is rising to 3.3V
While Vref_B is turned on and the voltage is rising to 3.3V (during the period below), what is the state of port B of LSF0204?
SignalA2 is driven low by the source device before Vref_B is turned on. I want to specifically check if Signal_B2 can stay low during the period when Vref_B is rising.
Vref_B = 0V
0V < Vref_B < Vref_A
Vref_A < Vref_B < Vref_A+0.8V
Application circuit
*Vref_B(3.3V) turns on after Vref_A(1.8V) turns on completely.