This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: Replicate 1 RX port

Part Number: DS90UB960-Q1

Hi,

We have 4 camera inputs to the 960. We need all 4 to be output on TX0 and 1 of them to be output on TX1. Is this possible with replicate or does replicate require the outputs on both TX ports to be the same?

Thanks,

Katie

  • Hello Katie,

    The UB960 does not support this kind of replication. Best solution is replicate all 4 on both TX ports, and the SoC will take the required RX port data (based on VC ID) and just leave the rest.
    Otherwise, you may want to use the 9702 and use exclusive forwarding