Hello ,
am working on a two-wheeler automotive application using a CAN bus. Normally, CAN requires a 120 Ohm termination at each end of the bus. In my design, the ECU may sometimes be at the end of the bus and sometimes in the middle, so I want to enable or disable termination dynamically via software (using a GPIO or similar).
My requirements:
- Automotive-grade solution (AEC-Q100/Q200 components)
- Must handle ISO 11898 CAN fault conditions and ESD/load dump
- Prefer split termination for EMC (two 60 Ohm capacitor)
- Looking for a low-cost solution
- Low power and compact (avoid mechanical relays if possible)
Questions:
- What is the best way to implement switchable termination in hardware for automotive CAN?
- Are there CAN transceivers with built-in termination control pins?
- If not, what analog switches or MOSFET-based solutions are recommended for automotive environments?
Any schematic examples or part recommendations would be helpful.