Part Number: DS90UB954-Q1
Hi Team,
Posting on behalf of our customer.
We have found in the UB954A datasheet that it supports the duplication of MIPI for parallel processing. For our parallel processing, we’re planning for the below architecture.
Plan A:

So we have few queries related to the same.
1. Does the above mentioned diagram will create any I2C conflicts?. Is it possible to assign the I2C address using Register settings. If so, please suggest possible values. Also, please suggest the possible I2C address via HW settings.
2. How much delay does the Intermediate Deser-Ser introduce in the MIPI path?
3. Can I use an MCU to configure the registers of Intermediate Deser-Ser chipsets, rather than depending on SoC1/SoC2?
Plan B:
We have also prepared another architecture, without using an MCU for the register configuration. Please refer to the 2nd diagram attached below.

So here also, we have similar queries, as mentioned earlier.
1. Does the above mentioned diagram will create any I2C conflicts?. Is it possible to assign the I2C address using Register settings. If so, please suggest possible values. Also, please suggest the possible I2C address via HW settings.
2. How much delay does the Intermediate Deser-Ser introduce in the MIPI path?
3. Can you suggest a register configuration sequence for the Serializer and Deserializers by avoiding possible register conflicts, if any
Could you please review the architecture and let us know whether the proposed design will work as expected, or if any additional changes are required? Your input during this architectural review phase is greatly appreciated. Also, kindly respond to the queries we have raised.
Regards,
Danilo