Part Number: TUSB7340
Dear Staff,
We're using TUSB7340 in our design, operating system is LINUX 6.1.112.
Also,The "TUSB7340" and "Vender:TI" can be identified using the command “lspci ”.
But, when plug in the USB 2.0 device, return the error as follow:
{
root@ubuntu:~# [ 1066.580657] usb 1-1: device descriptor read/64, error -71
[ 1066.884662] usb 1-1: device descriptor read/64, error -71
[ 1067.384665] usb 1-1: device descriptor read/64, error -71
[ 1067.688791] usb 1-1: device descriptor read/64, error -71
[ 1068.692644] usb 1-1: device not accepting address 8, error -71
[ 1069.304651] usb 1-1: device not accepting address 9, error -71
[ 1069.304734] usb usb1-port1: unable to enumerate USB device
}
Could you please help us review the SCH, and give some advices?