Part Number: AM62L
Hello ,
I had flashed uboot binaries using DFU and then followed the steps to flash the .wic file as mentioned in the below thread https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1596268/am62l-emmc-booting-issue-through-wic-file/6166947
tiny image .wic file is successfully flashed . But after observing the uboot binaries arent from the .wic file which i flashed these are from the previous binaries which i flashed through dfu tool.
i tried replacing the binaries using ums 0 mmc 0 command binaries are replaced but while booting these binaries arent used .
How to update the uboot binaries (tiboot3.bin tispl.bin u-boot.img ) which are used for booting ?
If there is any log or steps for reference to check the flashing and booting from .wic file ?
Thank you