In the slls684e.pdf is the specification/datasheet for the TPD2E001. It also specifies the recommended parts RT and C. Unfurtunately it does not give all required values for these parts not parts that are recommended as starting point. Are the following parts correct? Or is there a better part that we should be using:
RT, we image something like 1, 27 or 100 Ohms but don't know this for sure, SMD style. We are not sure what the value is and if there are additional requirements with respect to wattage for example.
C, at 0.1 micro F, probably should be rated at 200 V (100+VCC plus some arbitrary margin with minimum of 125V), ceramic. Mutlicomp MCCA000819 may be a good part. ???
The guide is straight forward but does not hint to design guides besides the DZD pad sizes. It would be nice to see what is the best layout because this is a critical element for us. Placing of RT and C and relative to connector and ground plane may be very important elements but there is not detail in the PDF on this. We are using EAGLE 6 and made a first draft part but know that this may not be enough.