This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65ALS180: Special Impedance for layout

Part Number: SN65ALS180

Is there any special impedance for layout or standard can be follwed? can you please confirm is standard 120 ohm 

  • Hi Nishalini,

    We are currently on a holiday. Please give until next week for an update, thanks.

    Best Regards,

    Michael.

  • Hi Nishalini,

    Impedance match should match the transmission line. This depends on the cable you use. For RS485, it is more common to have impedance controller cables of 120 ohm. Some cables have impedances of 100 ohms which is more common with RS422 systems. 

    3074F Technical Data Sheet

    An example of a cable above. You can look at the nominal impedance value in the datasheet of the cable which shows 120. If you know your cable for your system, then you should impedance match the traces to match that value.

    I also recommend you match the length of the traces for the A/B pins since these are differential pins.

    -Bobby