Part Number: SN65DP159
Hi TI Support Team,
We are using the SN65DP159 on a custom COM Express Type-6 carrier board to provide an HDMI output.
Under Linux, the HDMI output works correctly at 1920×1080 resolution.
However, under Windows 10, when the Intel graphics driver (31.x) is installed, the HDMI output does not work.
What we see:
-
In Windows Safe Mode or when using the Microsoft Basic Display Adapter, video output works.
-
When the Intel graphics driver is active, windows does not detect any physical HDMI monitor. Only a virtual display (for example, TeamViewer virtual monitor) is shown.
-
Booting Windows with the HDMI cable disconnected does not change the behavior.
-
We bypassed the ferrite beads on the DDC lines for testing, but there was no change.
Questions:
-
Have you seen cases where HDMI works on Linux but fails on Windows when using SN65DP159?
- During HDMI initialization, does the Intel Windows graphics driver expect any specific behavior from the redriver that differs from Linux drivers?
-
Can SN65DP159 load or bias the TMDS lines in a way that may cause the GPU HDMI initialization to fail, even without a monitor connected?
-
Can an incorrect TMDS lane order or polarity cause some operating systems to fail completely?
-
Is there any recommended enable or power-up sequence for SN65DP159 that could affect HDMI initialization?
-
For debugging, do you recommend bypassing the SN65DP159 to confirm whether it is the root cause?
We would like to know how to continue.
Best regards,
Ahmet