Part Number: TUSB320LAI
Good morning,
I need to connect a USB-C port to my system. My board needs to be programmed before being installed in the target cabinet, and I wanted to do this via the USB-C port.
My problem is that I need to power the microcontroller and the surrounding analog circuitry with the USB-C port. The combined current draw for 5V is about 2.5 amps. I'd like to use the TUSB320LAI in UFP mode. Additionally, for communication with the microcontroller, I'll use an FT232RN for USB-to-UART.
I wanted to know if I can get this much power from the power source (PC) I'll connect with the TUSB320LAI?
Is it also possible to request 5V 3A power without using the I2C/GPIO on the chip?
Thanks
Luca