Part Number: SN74AXC4T774
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AXC4T774
Hello Scott,
The issue you may be experiencing could be bus contention. The SN74AXC4T774 has integrated input pull-down resistors meaning if you leave the inputs floating, the output will always send a low signal.
For example, if SPI Slave 1 is sending MISO to the SPI Master, this line will be pulled low by both SPI Slave 2 and Aardbark level translators (even if both are idle). If this is the case then I would recommend forcing /OE pin high on all level translators not in use.
If bus contention is not the issue, then I would recommend probing the SPI bus to figure out why both AXC4Ts cannot work together.
Regards,
Josh