Part Number: TXV0106
Other Parts Discussed in Thread: SN74AXC8T245, , SN74AVC8T245
Dear Ladies and Gentlemans,
do you have more accureated values for VIL, VIH, VOH and VOL for different supply voltage like SN74AXC8T245 and SN74AVC8T245. I use a RGMII switch with 3,3V RGMII logic level and the CPU uses 1,8V level. The switch has VOHmin according the datasheet 2,1V and the TXV0106 has VIHmin accourding datasheet 0,7xVCC (2,31V @3,3V (for 1,14V-3,6V). Can I use TXV0106 or must i switch to SN74AXC8T245 or SN74AVC8T245. Thanks in advance!!
On other point is the drawing on page 1 on the datasheet is maybe wrong. Port A is Input and port B is output. TX -->Port A Port B--> RX, RX<--PortB <--Port A <--TX.