Part Number: TUSB8041
Hi Team,
I am using TUSB8041IPAPQ1 HUB for gateway project. I have one source USB 3.0 and USB 2.0 Ports. pls find the block diagram for the same below,
One output port of USB HUB USB 3.0 port connected to USB Type A connector and another USB 3.0 is connected to 5G cellular module from telit.
But, TYPE A USB 3.0 port alone is working meanwhile 5G cellular module is not working. Port is not seen in the system. we unable to get the USB ports for the 5G module.
We have tired removing the USB3.0 signals from USB type A connector and bypassed and connected to 5G Module, then 5G module USB is detected and working.
Thus, Pls suggest have we missing anything why another USB3.0 port is not working. do we need to do any configiuration in the HUB.?