Other Parts Discussed in Thread: ADC3669EVM,
Hello,
I have the setup ADC3669EVM + TSWDC155EVM somewhat functional using the provided excellent software support via HSDC-Pro-v5.31. However, I would like to use this setup for further evaluation with Python or LabVIEW example to stream data out for analysis.
BTW, The ADC3669EVM is a dual channel product. I can only see Channel A functional when I connect 10MHz to it and I switch 10MHz to Channel B I don't see any signal on the HSDC Pro v5.31 GUI.
Also, when I click on the "Configure" on the ADC3669EVM GUI I am getting following error shown under details:
"Traceback (most recent call last):
File "guilite_ps6\hsc_gui_lite.py", line 1974, in call
File "guilite_ps6\hsc_gui_lite.py", line 592, in __init__
AttributeError: 'Configuration_Window' object has no attribute 'titleBarText'
"
Please provide instructions of example code so I can utilize this fantastic HW setup for my application.
Thanks,
Iqbal